Technical FAQs

Ask a Question

SNMP Device Crawlers Targets Show Offline or Unavailable

Issue:

SNMP Device Crawlers Targets Show Offline or Unavailable

Product Line:

NetBotz

Environment:

NetBotz version 2 SNMP Device Crawlers

Cause:

Device Crawlers or Advanced Device Crawlers generally show an unavailable status on a device for one of the following reasons

Resolution:


- No connectivity between the bot and the device
- No SNMP agent installed
- Wrong community name
Was this helpful?
What can we do to improve the information ?