Technical FAQs
Technical FAQs
Issue
What are the recommended front and rear clearances for the installation of a single phase Symmetra UPS system that is in tower form factor?
Product Line
Symmetra LX
Symmetra Power Array
Environment
All serial ranges
Cause
To ensure proper airflow and access for maintenance, Symmetra LX should be installed with the proper front and rear clearances.
Resolution
The recommended front clearance is 48" and the recommended rear clearance is 12". There is no recommendation for side clearance as long as there is access to the front and rear of the system for maintenance.