Technical FAQs

Ask a Question

Video: Data Center Expert | How can I export data?

Process for exporting data from StruxureWare Data Center Expert.

Product Line:
StruxureWare Data Center Expert (DCE) 
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)

StruxureWare Data Center Expert (All Versions)


Information can be exported from Data Center Expert using the DCE Desktop Client or SOAP Web Services.
Exporting Data from the DCE Desktop Client

NOTE: Certain panes within the DCE Desktop Client have an export option.

An example of how to export all devices from the DCE Desktop Client:

1) Log into the DCE Desktop Client.

2) Open the Monitoring perspective.

3) Within the Device Group pane, click on All Devices.
NOTE: You can select a different group to export just those devices.
NOTE: You can search for devices using the search bar within the Device View pane to filter what devices to export.

4) In the upper-right corner of the device view pane, select the folder with the green arrow on it.
NOTE: Selecting the drop down will allow for export as a CSV or TXT file.
NOTE: Only the columns that are currently being displayed will be exported.

5) Save the file and open in a program that can open the type of file you chose to save.

Exporting Data Using SOAP Web Services

For information on pulling data from DCE using web services, visit DCIM Support.
Was this helpful?
What can we do to improve the information ?