Technical FAQs
Technical FAQs
Problem and Possible Cause | Solution |
The Back-UPS will not switch on | |
The Back-UPS is not connected to AC power | Ensure that the Back-UPS is securely connected to an AC outlet. |
The circuit breaker has been tripped. | Disconnect non-essential equipment from the Back-UPS. Reset the circuit breaker. Re-connect equipment one item at a time. If the circuit breaker is tripped again, disconnect the device that caused the trip. |
The internal battery is not connected. | Connect the battery. |
The AC input voltage is out of range. | Adjust the transfer voltage and sensitivity range. |
The Back-UPS does not provide power during a AC power outage. | |
Ensure that essential equipment is not plugged into a SURGE ONLY outlet. | Disconnect equipment from the SURGE ONLY outlet and re-connect to a Battery Backup outlet. |
The Back-UPS is operating on battery power, while connected to AC power. | |
The plug has partially pulled out of the wall outlet, the wall outlet is no longer receiving AC power, or the circuit breaker has been tripped. | Ensure that the plug is fully inserted into the wall outlet. Ensure that the wall outlet is receiving AC power by checking it with another device. |
The Back-UPS is performing an automatic self test. | No action is necessary. |
The AC input voltage is out of range, the frequency is out of range, or the waveform is distorted. | Adjust the transfer voltage and sensitivity range |
The Back-UPS does not provide the expected amount of backup time. | |
Battery Backup outlets may be fully or improperly loaded. | Disconnect non-essential equipment from the Battery Backup outlets and connect the equipment to SURGE outlets. |
The battery was recently discharged due to a power outage and has not fully recharged. | Charge the battery cartridge for 16 hours. |
The battery has reached the end of its useful life. | Replace the battery.
|
The REPLACE BATTERY indicator is illuminated. | |
The battery has reached the end of its useful life. | Replace the battery as early as possible.
|
The Building Wiring Fault LED illuminates | |
The building wiring presents a shock hazard that must be corrected by a qualified electrical. | Do not operate the Back-UPS. Call a qualified electrician to correct the building wiring fault. |
The OVERLOAD indicator is illuminated. | |
The equipment connected to the Back-UPS is drawing more power than the Back-UPS can provide | Disconnect non-essential equipment from the Battery Backup outlets and connect the equipment to SURGE outlets. |
The SYSTEM ERROR indicator is illuminated, all the front panel indicators are flashing. | |
There is an internal error. | Determine which internal error message is displayed by matching the number displayed on the LCD with the corresponding Error Message (see "System Errors") and contact SEIT Technical Support. |
System Errors; | |
F01 On-Battery Overload | Turn the Back-UPS off. Disconnect non-essential equipment from the Battery Backup outlets and the turn Back-UPS on. |
F02 On-Battery Output Short | Turn the Back-UPS off. Disconnect all equipment from the Battery Backup outlets and the turn Back-UPS on. Re-connect equipment one item at a time. If the output is tripped again, disconnect the device that caused the error. |
F03 On-Battery Xcap Overload F04 Clamp Short F05 Charge Error F06 Relay Welding F07 Temperature F09 Internal Error |
Errors F03-F09 cannot be corrected by the user, contact SEIT Technical Support for assistance. |