How do you read the color code on the IDC connectors of the Cat 6 Patch Panels?
Issue:
Customers may question which color code instructions to follow, 568B vs. 568A. Or they may not understand how to read the color code.
Product Line:
Cables and Connectivity Solutions, Cat 6 Patch Panels
Environment:
All versions and serial ranges.
Cause:
The color code instructions may be confusing.
Resolution:
For high speed networking 568B is used almost universally.
If you need help determining how to terminate to the 568B or 568A color code please see the attached file.