Technical FAQs

Ask a Question

Can I use the NetBotz leak rope sensors with the Network Air units?

Issue:

NetBotz leak rope sensors can not be used with Network air units.

Product Line:

NetBotz

Environment:

NetBotz version 3 and leak rope sensors NBES0308 and NBES0308

Cause:

NetBotz leak rope sensors NBES0308 and NBES0308 have specific resistances that are expected by the NetBotz appliance.

Resolution:

The leak rope sensors AP9325 and AP9326 are designed specifically for the APC Network Air units they work with, You can not use these sensors on a NetBotz appliance nor can you use the NetBotz NBES0308 and NBES0308 rope leak sensors with APC's Air units.
 
Was this helpful?
What can we do to improve the information ?