Technical FAQs

Ask a Question

How much extra space is there to the front and rear of the internal rack posts on the NetShelter CX when the rails are at their furthest positions?

Issue:
Customers need to know how much room there is in the NetShelter CX beyond the rails.

Product Line:
NetShelter CX
 
Environment:
All versions and serial ranges.
 
Cause:
Customers want to avoid interference with the front door and rear fan units.
 
Resolution: 
Forward of the front rack posts = 100mm / 4”
Rearward of the rear rack posts = 60mm / 2” (Except, where fan modules intrude there is no usable extra space)
 
Was this helpful?
What can we do to improve the information ?