Technical FAQs

Ask a Question

Upgrading to PowerChute Personal Edition v3.X on Vista: “Program might not have installed correctly”

Issue:
Upgrading to PowerChute Personal Edition v3.X on Vista: “Program might not have installed correctly”

Product:
PowerChute Personal Edition version 3.X

Environment:
Windows Vista

Cause:
When you cancel an upgrade to PowerChute v3.X on Windows Vista, an error message will state: "The program might not have installed correctly".

 Solution:

This is a harmless message and you can continue to use the currently installed version of PowerChute Personal Edition.

Was this helpful?
What can we do to improve the information ?