Technical FAQs

Ask a Question

Is there a roof available for the AR3100 which is solid and does not have open cable access holes?

Customers may need for a solid roof on their cabinets.

Product Line:
NetShelter SX
All versions and serial ranges.
A more secure roof may be required for installations such as PCI.
The WAR7210 can be used where high security is required. It is compatible with the following models: AR3100, AR3104, AR3105, AR3200 and AR3107.
For more information and a photo please see the attached file.
Was this helpful?
What can we do to improve the information ?