InfrastruXure Central 6.0 dialog buttons do not work with mouse in latest versions of linux
Issue:
InfrastruXure Central 6.0 dialog buttons do not work with mouse in latest versions of linux
Product Line:
InfraStruXure Central
Environment:
InfraStruXure Central 6.0
Cause:
It has been noticed in recent Linux updates, notably Fedora 12 and Ubuntu 9.10, that users are unable to use the mouse to click on dialog buttons within the user interface.
Resolution:
Upgrading to version 6.2 or later will resolve this issue. If 6.0 must continue to be used with the affected operating systems, a simple workaround is to use the keyboard to select dialog buttons when navigating the InfraStruXure Central 6.0 user interface.