FIJI - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
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
Data Center Assessment Services
Install
Installation Services
Operate
Remote Monitoring Services
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
FIJI - Choose Country or Region
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
USB CAT-5 Pod Extender Specifications
Issue:
USB CAT-5 Pod Extender Specifications
Product Line:
NetBotz
Environment:
NetBotz CAT5 pod extender
Cause:
Configuration.
Resolution:
The NetBotz CAT-5 Pod Extender is composed of two main components:
Local Extender Unit
Remote Extender Unit
There are two versions of the NetBotz CAT-5 Pod Extender:
Model 110i - which has 1 USB port on the remote end
Model 410i - which has 4 USB ports on the remote end
The NetBotz CAT-5 Pod Extenders support up to 330 feet of CAT-5 cabling between the local and remote ends.
Local Extender Unit:
Self-powered
Attaches to NetBotz 420 or 500 via standard USB cable
Upstream = USB “B” connector (connects to the 420 or 500)
Downstream = RJ-45 connector (connects to the Remote Extender Unit)
Remote Extender Unit:
Self-powered
Integrated 1 port USB hub
Upstream = RJ-45 connector (connects to the Local Extender Unit)
Downstream = USB “A” connector(s) (connects to camera or sensor pods)
Maximum of 1 hub can be connected to the Remote Extender Unit to extend an additional 16 feet or 5 meters.
NOTE:
Only one end of the CAT-5 Pod Extender has to be powered. The power can be supplied to the Local or Remote Pod Extender.