Determining SSL Connection Information from the Netbotz Advanced View
Issue:
Determining SSL Connection Information from the Netbotz Advanced View
Product Line:
NetBotz
Environment:
NetBotz version 2
Cause:
The Advanced View does not provide SSL session and connection information. To see the SSL session and cipher information, additional logging parameters must be configured.
Resolution:
Edit the "NetBotz Advanced View.lax" file in directory where the Advanced View is installed.
Add the following line to the file:
lax.nl.java.option.additional=-Djavax.net.debug=ssl
Save the file and restart the Advanced View.
Now the Advanced View Log file in the "logs" subdirectory will contain the SSL session information.