Technical FAQs

Ask a Question

SUVT External Battery Frame

"The SUVT can be attached to External Battery Frames in order to increase the runtime.

The maximum number of External Battery Frames is limited to 4 due to the recharge time.

There are 2 different External Battery Frame models depending on whether the frame has Circuit Breaker integrated or not.

External Battery Frames for SUVT:

1-Battery Frames with Circuit Breaker:

SUVTBXR2B6S

SUVTBXR6B6S

2-Battery Frames without Circuit Breaker:

SUVTXR2B6S

SUVTXR6B6S


"
Was this helpful?
What can we do to improve the information ?