Technical FAQs

Ask a Question

What are the placement considerations for the fluid cooler relative to the InRow ACRD20x?

Issue:
What are the placement considerations for the fluid cooler relative to the InRow ACRD20x?

Product line:
ACRD200, ACRD201

Environment:
Data Center Cooling

Cause:

Resolution:
The fluid cooler can be placed up to 600ft equivalent pipe length from the unit. The fluid cooler may be placed at levels above or below the unit within the distance specified. The longer the distance of the fluid cooler from the indoor unit, the larger the size of the pump required. 
 
Was this helpful?
What can we do to improve the information ?