ETHIOPIA - Choose Country or Region
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
Voltage Regulators
Surge Protection Devices
Filters & Harmonic Conditioners
Mobile Accessories
Portable Device Chargers
Cooling
Cooling
Cooling
Modular Access Floor
Uniflair Technical Floor
Uniflair Office Floor
Uniflair Building Floor
Air Economizers
Ecoflair Air Economizers
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
Static Transfer Switches
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
Module Optimized Cooling
Chilled Water System
Power Modules
Enclosed Power Module
Skid Mounted Power Module
IT Modules
SmartShelter Container
SmartShelter Module
SmartShelter Data Hall
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
Data Center Assessment Services
Install
Installation Services
Operate
Battery Replacement Services
Extended Warranties
Preventive Maintenance
Service Plans
Optimize
Training Services
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
ETHIOPIA - Choose Country or Region
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
Polarity of 0-5V Sensor Cable NBCD0001
Issue:
Polarity of 0-5V Sensor Cable NBCD0001
Product Line:
NetBotz
Environment:
NetBotz version 1 and 2
NBCD0001
Cause:
Configuation / connection to 0-5v source.
Resolution:
One end of NetBotz 0-5V Sensor Cable is DIN6 (ps/2) connector, which goes to an external sensor port on 320/420/500 model or Sensor Pod 120. On the other end are 2 wires - the black wire is ground (-); the red is sense (+).