Technical FAQs

Ask a Question

Video: How to clear a latched alarm on an Smart ATS

Issue:
How to clear a latched alarm on an ATS
 
Product line:
APC ISX-ATS-GEN, SmartGen ATS
 
Environment:
All Product models, all serial numbers
 
Cause:
How to clear a latched alarm on an ATS

Resolution:
Go through the steps for clearing latched alarms on an APC ATS via the display:
 
  1. Select ‘Alarms’ from the main menu
  2. Select ‘Alarm/Event Log’ from the Alarms menu
  3. Select ‘Clear Latched Alarms’

You can also clear alarms by resetting the automatic operation on the ATS:
  1. Locate the Automatic Operation Switch on the ATS and turn it to Disable. 
  2. When the "Not in Automatic Operation" light illuminates, turn it back to Enable. The orange LED will be extinguished.

The following video demonstrates these procedures:
 
Was this helpful?
What can we do to improve the information ?