Technical FAQs

Ask a Question

What Proximity Cards are supported by the NetBotz NBACS125 & NBACS1356 Rack Access Control Systems?

The NBACS125 Rack Access Control appliance supports the following Proximity Cards
  • H10301 - Standard 26 Bit
  • H10302 - 37 Bit without facility code
  • H10304 - 37 Bit with facility code
  • CORP1000

    NBACS125 ships with 2 x Standard 26 Bit cards. Additional packs of 10 cards (AP9370-10) can by purchased from Schneider Electric.

The NBACS1356 Rack Access Control appliance supports the following Proximity Cards
  • MIFAREC4 - Mifare Classic 4 byte
  • MIFAREC7 - Mifare Classic 7 byte
  • MIFAREDF - Mifare DESfire
  • MIFAREPL - Mifare Plus
  • iClass support will be added in 2017

    NBACS1356 does not ship with any Proximity Cards. Schneider Electric does not sell these cards at this time.

For more information, see the product brochure below.

http://www.apc.com/salestools/MKEY-ADCS74/MKEY-ADCS74_R0_EN.pdf

Note: Pod Sharing with the NBACS125 / NBACS1356 Rack Access Control systems is NOT supported at this time
 
Was this helpful?
What can we do to improve the information ?