Technical FAQs

Ask a Question

What is the maximum roof load rating for NetShelter SX and SV cabinets?

The maximum load rating for the roof is needed.

Product Line:
NetShelter SX, NetShelter SV

All versions and serial ranges.

Customers need to know the load rating to make sure it's not exceeded.

The roof of both the NetShelter SX and SV cabinets is rated to 200 lbs.
Was this helpful?
What can we do to improve the information ?