Technical FAQs

Ask a Question

What is the minimum distance required between mounting rails in a NetShelter SX cabinet when installing the AR7725?

Issue:
Customers may want to know what distance is required between the NetShelter SX mounting rails to install the AR7725.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Knowing the minimum distance helps customers understand how much spare room there will be in the cabinet for installing cable management or PDUs.

Resolution:
The AR7725 requires 24.83" (630.68mm) distance between the NetShelter SX mounting rails to mount.
Was this helpful?
What can we do to improve the information ?