Are there Windows or Linux drivers for the NBAC0226 USB to serial cable.
Issue:
There are no drivers available for the NBAC0226 serial to USB cable.
Product Line:
NetBotz
Environment:
NetBotz Serial devices
Cause:
The NBAC0226 Is meant to connect certain serial devices to NetBotz appliances by means of their USB connection
Resolution:
This USB to serial converter is only meant to connect serial devices to a NetBotz appliance. It is not meant as a Windows or Linux Serial to USB converter. There are no drivers available for this cable.