Technical FAQs

Ask a Question

Details Returned from Foundry Devices via Advanced Device Crawlers

Issue:

Details Returned from Foundry Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Foundry systems assuming the Foundry DDF (Device Definition File) is installed on the NetBotz appliance and the Foundry device is SNMP enabled. Please note that not all information listed below is available on all Foundry models.

Resolution:

 
  • Chassis Temperature
  • Status
Was this helpful?
What can we do to improve the information ?