Technical FAQs

Ask a Question

Netbotz: Modifying or Changing Default Email Messages

Issue:

Netbotz: can not change default Email messages on version 1 appliance

Product Line:

NetBotz

Environment:

NetBotz version 1

Cause:

The default email notification can NOT be customized for Version 1 Appliances (300, 303, 310, 400).

Resolution:

As a workaround, using the "Short Message" capability customized emails can be sent from the Version 1 Appliances. The "Short Message" Configuration can be accessed via the Advanced View under "Network"->"Email". On the "Short Message" tab you can customize with Macros what data is inserted in the subject and body of the email.

Was this helpful?
What can we do to improve the information ?