Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)
Issue:
Using the Male to Male BNC Adapter Included in a Day/Night CCTV Camera (NBAC0224)
Product Line:
NetBotz
Environment:
NetBotz NBAC0224
Cause:
Physical configuration options.
Resolution:
The NetBotz Day/Night CCTV Camera has a BNC female output.
The NetBotz CCTV Pod has BNC connection that looks like a male connector but it actually has a hole in the male connection so it will accept the male-male adaptor included with a Day/Night CCTV Camera.