Technical FAQs

Ask a Question

What input supply changes are necessary to feed a 208v Symmetra LX 240 VAC?

Symmetra LX can automatically adjust to input voltage between 200 and 240 volts. No change to the system is required to accommodate these voltages.  However, it is best practice to set the output voltage and frequency to match the input voltage and frequency.  This will help avoid problems with bypass operation of the UPS.  These changes can be made via the front display or the network management card.

Was this helpful?
What can we do to improve the information ?