Technical FAQs

Ask a Question

Register Map For NetBotz 200 and 250 does not include external sensor pod sensors.

Issue:

Register Map For NetBotz 200 and 250 does not include external sensor pod sensors.

Product Line:

NetBotz

Environment:

NBRK0200
NBRK0250
NBPD0150
Modbus Output


Cause:

The modbus option was left out of the NetBotz 200 code. Since the code in the 250 was based on this code, this limitation is also seen in the NetBotz 250.

Resolution:

Currently there is no option to get the modbus output for the sensors connected to the external 150 pod. SNMP output will work fine for these sensors and if using StruxureWare DCE, you can use it's modbus output capabilities (with the AP95MODBUS license) to output the sensor pods for the 200 and 250. The 250 should have an update soon that allows for the modbus output.
 
Was this helpful?
What can we do to improve the information ?