Technical FAQs

Ask a Question

How to change Humidify and Dehumidify set points in a Uniflair unit.

Issue:
How to change Humidify and Dehumidify set points in a Uniflair unit.
 
Product line:
All Gen 1 Uniflairs with push button displays and all Chilled Water Uniflairs
 
Environment:
Push Button Display Uniflair units and all Chilled water Uniflair
 
Cause:
Install, Repair Maintenance
 
Resolution
 
How to change Humidity and Dehumidify set points
 
Press the PRG button
 
Press ENTER on the Settings Menu
 
Press ENTER on passcode if required 00000
 
Press ENTER on Operative settings
 
Use the Arrows to scroll to the Humidity Settings
 
Press the ENTER button to get to the desired setting that needs to be changed
 
Use the Arrows to change the settings
 
Press ENTER to go back to the top of the screen
 
Press ESC back to the main screen
 
 
 
 
Was this helpful?
What can we do to improve the information ?