Technical FAQs

Ask a Question

Video: How to set Units of Measure on an InRow ACRD200 cooling unit

Issue:
How set Units of Measure on an ACRD200 cooling unit

Product line:
ACRD200

Environment:
All Serial Numbers

Cause:
Install, Configuration

Resolution:



Press ESC until you get to the main screen (On/Standby)
 
Use the Up or Down arrows to find the heading Set Display Units
 
Press ENTER and select Units
 
Now you will be prompted for a password
 
Use the default password of “apc”
 
If this does not work check with your Admin for the correct password
 
If password has been lost use the last eight digits of the serial number
 
Press Enter and select between US and Metric
 
 
Was this helpful?
What can we do to improve the information ?