Video: How to take Silcon UPS out of Maintenance Bypass (MBP)
Issue:
How to take Silcon UPS out of Maintenance Bypass (MBP)
Product line:
Silcon
Environment:
All Product models, all serial numbers
Cause: This video provides a step by step instruction on how to operate the Silcon UPS from Maintenance Bypass mode, to allow the end-user to transfer load back onto the UPS, without interruption to their load.
Resolution:
Display will say Bypass Operation
The Green LED (H002) above Q002 will be illuminated; you can now turn Q002 to ON (Center)
The Green LED (H003) above Q003 on the bypass panel will be illuminated; you can now turn Q003 to off (Right)
Press # key
Use the arrow keys to scroll to Bypass Operation: Yes
Press the C key to change to Bypass Operation: No
Press # to store – Display will flash the message “Data Stored”
UPS will go to Normal operation
The Green LED (H002) above Q002 on the bypass panel will go off