Technical FAQs

Ask a Question

MGE SNMP Card 66074 or 34003640SE; Special characters can be used for password on a SNMP card

Issue:

Special characters can be used for password on a SNMP card

 

Product line:

SNMP card part#: 66074 or 34003640SE

All MGE UPS

 

Environment:

All model numbers/ all serial numbers

 

Cause:

Customer wanted to use special characters for password on a SNMP card for higher level of security. The login and password by default are: MGEUPS. Each field accepts up to 10 characters max.

 

Resolution:

Here are the special characters can be use for password ~ ! @ # $ % * ( )

 

 

 

Was this helpful?
What can we do to improve the information ?