Technical FAQs
Technical FAQs
Knowledge Base Article ID Resolved | Network Management Card AOS or APP Module Version Required |
FA175981, FA176048 | AOS v6.1.1 or higher |
FA175980 | AOS v6.1.3 or higher |
FA175982 | AOS v6.1.6 or higher |
FA170552 (and related to note in FA176542) | AOS v6.1.3 or higher |
FA177701 | AOS v6.1.3 or higher |
FA177263 | sy APP v6.2.0 or higher |
FA231396 | sumx APP v6.2.0 or higher |
FA233873 | rpdu2g APP v6.3.3 or higher |
FA234740 | sumx v6.3.3 or higher |
FA235265 | AOS v6.3.3 or higher |
FA235654 | AOS v6.3.3 or higher |
FA235716 | undetermined future version of sumx firmware APP |
FA238090 | under investigation for future version of sumx firmware APP |
FA241052 | v6.3.2 rpdu2g firmware APP |
FA242818 | language pack fix attached in knowledge base ID |
FA238115 | detailed fix information available in knowledge base ID |
FA243736 | undetermined version of sumx/sy APP, workaround available in knowledge base ID |