Technical FAQs

Ask a Question

Details Returned from Best Power Devices via Advanced Device Crawlers

Issue:

Details Returned from Best Power Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Best Power UPS systems assuming the Best Power DDF (Device Definition File) is installed on the NetBotz appliance and the Best Power UPS is SNMP enabled. Please note that not all information listed below is available on all Best Power models.

Resolution:


  • Description
  • Battery Status
  • Time on Battery
  • Battery Runtime Remaining
  • Battery Voltage
  • Battery Current
  • Internal UPS Temperature
  • Battery Cell Voltage
  • Battery Positive Voltage
  • Battery Negative Voltage
  • Utility Line Input Frequency
  • Utility Line Input Voltage
  • Utility Line Input Current
  • 3-Phase Input Current
  • 3-Phase Input Voltage
  • Output Frequency
  • Output Voltage
  • Output Current
  • True Output Power
  • Apparent Output Power
  • Output Power Factor
  • Percent Full Load
  • Number of Active Alarm Conditions
  • Last Known Alarm
  • UPS Bypass Status
  • 3-Phase Output Voltage
  • 3-Phase Output Current
  • 3-Phase Apparent Output Power
  • 3-Phase True Output Power
  • 3-Phase Output Power Factor
  • 3-Phase Output Percent Load
  • 3-Phase Bypass Voltage
Was this helpful?
What can we do to improve the information ?