Eliminating Multiple Alert Notifications from NetBotz appliances
Product Line:
NetBotz
Environment:
Potentially any version
Cause:
Potentially, different configuration options may cause repeated alerts.
Resolution:
- Check that each alert action associated with an alert sequence does not have duplicate addresses associated with it.
- Verify that the different alert sequences within a profile is not set up with the same notifications.
- Thresholds may have a threshold specific e-mail address associated with it. Make sure this is not a duplicate of an address already associated with the actions.
- Make sure the threshold is not set up so that the threshold itself is switching into and out of alert too frequently.
- Increase the notification interval or decrease the number of notifications in the Alert configuration / profile
- Maks sure the check box is unchecked for"Automatically add new alert actions to this schedule" for any alert profile sequences.