Technical FAQs

Ask a Question

Notification when NetBotz Central runs out of appliance or Surveillance licenses

Issue:

Notification when NetBotz Central runs out of appliance or Surveillance licenses

Product Line:

NetBotz Central

Environment:

NetBotz Central 2.x

Cause:

Reaching licensing limits.

Resolution:

When an additional appliance is added to NetBotz Central or an additional appliance is attempted to licensed for Surveillance and if the NetBotz Central has all available licenses consumed, the system will provide feedback to the user indicating that no more licenses are available.
Was this helpful?
What can we do to improve the information ?