Technical FAQs

Ask a Question

Can I access the condenser fans from the front only on the ACSC unit?

Issue:
Can I access the condenser fans from the front only?
 
Product line:
ACSC100, ACSC101

Environment:
InRow Cooling
 
Cause:
 
Resolution:
Yes. Side access makes the job easier, but the condenser fans can be serviced from the front.
Was this helpful?
What can we do to improve the information ?