Technical FAQs

Ask a Question

What are the default Thresholds for Version 2 Appliances?

Issue:

Default Thresholds for NetBotz Version 2 Appliance

Product Line:

NetBotz

Environment:

NetBotz Version 2 Appliances

Cause:

Default configurations

Resolution:

Default Thresholds for Version 2 Appliances

The follow are the default thresholds on Version 2 Appliances (320, 420, 500):

Airflow:

-35 feet per minute for 60 seconds
-10.6 meters per minute for 60 seconds

**********************
Audio:

-40 for 30 seconds

*************************************
Dew Point:

-maximum 64.4 F & minimum 28.4 F
-maximum 18 C & minimum 2 C

*************************************

Humidity:

-maximum 50%
-minimum 20%

**********************************
Temperature:

-maximum 80 F
-minimum 68 F

-maximum 26.6 C
-minimum 20 C

***********************************
Was this helpful?
What can we do to improve the information ?