Technical FAQs

Ask a Question

Daisy Chaining Netbotz Door Switch Sensors

Issue:

Daisy Chaining Netbotz Door Switch Sensors

Product Line:

NetBotz

Environment:

NetBotz door sensors

Cause:

Alternative configurations.

Resolution:

It is possible to daisy chain door sensors. When door switches are chained together the system will not be able to identify which door opened, only that "a" door opened. The attached PDF outlines how to wire the contacts together.

Note: This does require cutting and splicing of wires
 
Was this helpful?
What can we do to improve the information ?