Maximum Number of Netbotz Appliances or Sensors on a Graph within Netbotz Central.
Issue:
Maximum Number of Netbotz Appliances or Sensors on a Graph within Netbotz Central
Product Line:
Netbotz Central
Environment:
NetBotz Central 1.x and 2.x
Cause:
Software Limitations.
Resolution:
Maximum Number of Appliances or Sensors on a Graph
NetBotz Central 1.x only graph 11 appliances at once. If more than 11 appliances are selected, then only first 11 selected are graphed.
NetBotz Central 2.x does not have this limitation. It can generate graphs for different sensors of the same type for a single appliance or multiple appliances. However, the more sensors are selected for a graph, the more memory and processing power are required for the client running NetBotz Central console.