* Ensure that Network Interfaces and DNS information is complete and correct
* Ensure the Region and Clock settings are complete and correct
* Upgrade the appliance to the latest available version of firmware / BotzWare
* Provide descriptive / unique name for the appliance in the Location configuration
* Change Camera Visual Mode to Widescreen
* Configure the Email Server settings
* Change the NetBotz User password
* Change the Root User password
* Configure sensor thresholds
* Configure camera capture settings
* Configure alert actions
* Test alert actions
* Backup the appliance configuration