"Manually rotate units in RUG use the following path in the unit addresses as the 1 unit: Path: Config >> Enter >> Enter (curser at Custom Setup) >> Down Arrow >> Scroll to Page 21 >> Special
Toggle through units in a Shared Display setup: Path: Help and Network buttons at the same time
Resetting/Reconfiguring Board Path: Blank Button >> enter (curser will move to the model above Software) >> Temp. and Run Hours at the same time (curser will move below the Software Ver. # >> Down arrow >> enter
Back Door Password Path: Blank button >> Network and Temp. at the same time >> Down arrow >> this will take you to the section where you can view or alter the 2 level passwords
Factory Menu Path: Blank button >> Config. >> Enter >> Enter (Curser should be at the Custom Setup) >> Special and Config at the same time
Clearing Alarm History Path: Alarm History >> Blank Button >> Help
Addressing the Board to the Display Path: Temp & Humid & Run Hours simultaneously "