DOMINICA - Choose Country or Region
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
Audio-Video Solutions
AV Power Conditioners with Battery
AV Surge Protectors
AV Power Filters
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
Room Cooling Accessories
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
iBusway for Data Center
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
Room Power Distribution
Cabinet Power Distribution
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
SmartShelter Room
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
Remote Monitoring Services
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
When to replace your battery or UPS
UPS Buying Guide
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
DOMINICA - Choose Country or Region
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
How quiet (or noisy) is the NetShelter CX when only the fans are running, with no equipment installed?
Issue:
Customer wants to know how quiet the cabinet is with nothing installed, just the fans running.
Product Line:
NetShelter CX
Environment:
All versions and serial ranges.
Cause:
Noise reduction in the office is important.
Resolution:
Noise of AR4018A / AR4018IA:
40.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
Noise of AR4024A / AR4024IA:
43.0 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet
Noise of AR4038A / AR4838IA:
43.5 dBA total noise generated, measured 1.0 m / 39" in front of the cabinet