Technical FAQs

Ask a Question

MGE EPS 6,7,8k Installation, Technical Specs and Operation Manuals

 
Issue:
MGE EPS 6,7,8k Installation, Technical Specs and Operation Manuals
 
Product line:
EPS 6000
EPS 7000
EPS 8000
 
Environment:
Customers and Sales Reps asking for Installation, Technical Specs and Operation Manuals
 
Cause:
Customer or sales rep are unable to find the documentation with their UPS
 
Resolution:
Provide the following links to customer for Installation, Technical Specs and Operation Manuals
 
EPS 8000
http://www.apc.com/shop/us/en/products/MGE-EPS-8000-800-kVA/P-E8TUPS800
 
EPS 7000
http://www.apc.com/shop/us/en/products/MGE-EPS-7000-500-kVA/P-E7TUPS500
 
EPS 6000
http://www.apc.com/shop/us/en/products/EPS-6000-625-kVA/P-E6TUPS625
 
If the customer or sales rep is looking for specific drawings for Qsku, 99-xxxxxx-xx and other customer products than Lvl2 or TTL will need to get involved.
 

 
Was this helpful?
What can we do to improve the information ?