Technical FAQs

Ask a Question

Do we offer a grounding cage nut?

Issue:
There are cage nuts made that can ground equipment chassis to the cabinet's rails.

Product Line:
NetShelter

Environment:
All versions and serial ranges.

Cause:
Customer inquires about grounded cage nuts.

Resolution:
We do not currently offer a grounded cage nut.
A better solution is to use AR8395 copper busbar, and connect a ground wire from the equipment's chassis ground points directly to the busbar. This makes a more reliable contact.
Was this helpful?
What can we do to improve the information ?