Technical FAQs

Ask a Question

How are the vertical mounting rails (PMA) oriented in the NetShelter cabinets?

A customer need to purchase a replacement vertical mounting rail and needs to know if they should order a Left Hand rail or a Right Hand rail.

Product Line:
NetShelter SX, SV, VX

All versions and serial ranges.

The description of the rails read "Left Hand" and "Right Hand". The description doesn't specify 'front' or 'rear'.

Please see attached file.
Was this helpful?
What can we do to improve the information ?