Technical FAQs

Ask a Question

ACPSC2000/3500 Spare Parts List

Issue:
ACPSC2000/3500 Spare Parts List 

Product line:
ACPSC2000/3500 

Environment:
Data Center Cooling 

Cause: 

Resolution:

Please contact Cooling Tech Support to confirm the part numbers before quoting as some may have changed. 888-695-6500 Option 2, Option 2, Option 2

 


Caster Wheels             0J-870-16521              This comes with four casters
Ducting Kit                   0J-0H-0308
Ceiling Kit                    0J-0H-0307
Air Filter                      0J-876-0318

Was this helpful?
What can we do to improve the information ?