Technical FAQs

Ask a Question

How many leak sensor cables can be attached in series on any 300 mm units.


                                                                                                                                                           

Issue:  How many leak sensor cables can be attached in series on any 300 mm units.

 

Product line: All 300 mm units

 

Environment:  All Serials

 

 

Cause:  Install

  

 

Resolution:

 

 

Leak detector port

Rope water detector (AP9325). Up to four optional rope water detectors can be installed in series. The rope water detector connects to the RJ45 leak detector port located at the top of the interface box.

 

 

Was this helpful?
What can we do to improve the information ?