DOMINICA - Choose Country or Region
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
Audio-Video Solutions
AV Power Conditioners with Battery
AV Surge Protectors
AV Power Filters
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
Room Cooling Accessories
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
iBusway for Data Center
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
Room Power Distribution
Cabinet Power Distribution
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
SmartShelter Room
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
Remote Monitoring Services
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
When to replace your battery or UPS
UPS Buying Guide
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
DOMINICA - Choose Country or Region
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
PowerChute Business Edition events are not being logged to the Windows Application Log.
Issue:
PowerChute Business Edition events are not being logged to the Windows Application Log.
Product Line:
PowerChute Business Edition, prior to v9.1.1
Environment:
All supported Windows OS with Java versions
7 update 21 or later
6 update 45
5 update 45
Cause:
Changes by Oracle to latest Java versions
Solution:
Upgrade PowerChute to the latest version available at this link
http://www.apc.com/us/en/faqs/FA304446/
NOTE:
If you are running a version of PowerChute Agent prior to 9.1.1, and you use the JRE Configuration Tool to upgrade to a JRE version HIGHER than any of the following, PowerChute stops writing events to the Windows application log:
Java 7 update 21
Java 6 update 45
Java 5 update 45