Technical FAQs

Ask a Question

Details Returned from Mitsubishi Devices via Advanced Device Crawlers

Issue:

Details Returned from Mitsubishi Devices via Advanced Device Crawlers

Product Line:

NetBotz

Environment:

NetBotz version 2 Advanced Device Crawlers.

Cause:

The following information can be queried via Advanced Device Crawlers for Mitsubishi UPS systems assuming the Mitsubishi DDF (Device Definition File) is installed on the NetBotz appliance and the Mitsubishi UPS is SNMP enabled. Please note that not all information listed below is available on all Mitsubishi UPS models.

Resolution:


 
  • Vendor
  • Description
  • Battery Status
  • Time On Battery
  • Battery Run Time Remaining
  • Remaining Battery Capacity
  • Battery Voltage
  • Battery Current
  • Battery Temperature
  • Input Line Voltage
  • Input Line Current
  • Input Line True Power
  • Output Source
  • Output Frequency
  • Output Line Current
  • Output Line True Power
  • Output Line Current Load
  • Bypass Frequency
  • Bypass Line Current
  • Bypass Line True Power
Was this helpful?
What can we do to improve the information ?