Technical FAQs

Ask a Question

NetBotz v2 | Contents of the Mounting Kit Included with the Models 320 & 420

Issue:
Contents of the Mounting Kit Included with the Models 320 & 420

Product Line:
NetBotz v2 (NB)

Environment:
NetBotz (320 & 420)

Resolution:

The following items are included in the mounting kits:
- Black universal swivel wall mount (plastic)
- 3 anchors (1"" long)(suitable for concrete) and 3 anchors (1-1/2"" long)(for sheet rock).
- 4 screws (#6 x 1/4"", phillips)
- 5 black tie wraps (7-1/2"" long) and 4 platforms (adhesive; can be stuck on walls; used with the tie wraps). 
Was this helpful?
What can we do to improve the information ?