Technical FAQs
Technical FAQs
Issue
I need to install or replace a module in my Symmetra Power Array UPS system. How do I do this?
Product Line
Symmetra Power Array
Environment
All serial ranges
Cause
Symmetra UPS are designed with modularity so that modules can be added or replaced as needed. This document contains a video to aid the user in performing the installation of a new module or replacement of an existing module.
Resolution
The following videos detail the process of replacing the Intelligence, Battery, and Power Modules in the Symmetra Power Array UPS.