Technical FAQs

Ask a Question

InRow Entering Fluid Temp threshold is not alarming

Issue:
InRow Entering Fluid Temp threshold is not alarming 
 
Product line:
InRow
 
Environment:
Data Center Cooling
 
Cause:
 
Resolution:
In the newest firmware ACRC 372 and higher the entering fluid temp alarm threshold violation will not be reported unless two conditions are met. The unit has a >=40% valve position opening , and the entering temperature is above the threshold.
Was this helpful?
What can we do to improve the information ?